Industry Online Support
Technical Forum
11/17/2009 4:36 AM | |
Posts: 7 Rating: (1) |
Hello, All experts, In my project I fell in a problem: We use 1 set Siemens PRIMERGY Tx150 S6 installed Windows 2003 Std Server SP2 and WinCC V6.2 SP2 and DataMonitor V6.2 ASIA (server+client options) as our OS server in control room, in work field in the remotepanel box we install 1 set SIMATIC thin client 15"(6AV6646-0AB21-2AX0) as theDat@Monitor client panel.TheWinCC project process pictures are designed as 1280*1024, but it was said that the thin client's physical resolution only support 1024*768. We 'd like the process pictures can automaticlly fitinto the1024*768 frame without any bar below and besidefor dragingpurpose. According to FAQ ID:5906788/19055678 I tried to use the 'FITTOSIZE=TRUE' parameter to manage to realize our purpose, but if I use it on computer IE screen(after change the resolution to 1024*768 first), with the mouse's rollerhelp I can managed to fit it to a suitable size. But there are no mouse roller I can use on the thin client, is there some method to solve this? How to realize the suitable picture size on the thin client? By the way, our project is pure WinCC project, not use the OS project editor to setup the frame works, our main framework is divided into three parts(Head, Process, Buttons), each time I need operate seperately for each part to change the picture size to fit the small frame. Any suggestion, pls send me emails. Thanks a lot. |
Last edited by: ccwwll at: 11/17/2009 4:39 AM |
|
1/7/2010 9:20 AM | |
Posts: 7 Rating: (1) |
??? |
Follow us on