Industry Online Support
Technical Forum
1/24/2010 9:42 AM | |
Posts: 101 Rating: (11) |
Does the sensor have the ability to connect to an RS232 port? if yes, you could think of an RF Transceiver. |
1/24/2010 3:43 PM | |
Joined: 5/4/2009 Last visit: 5/28/2024 Posts: 914 Rating: (40) |
Hello... No is does not hve the ability to be connected to RS-232. regards. Tomy. |
Aim Higher |
|
1/24/2010 3:54 PM | |
Posts: 2930 Rating: (432)
|
Hi, connect your sensor to a S7-200 PLC locally. Then you can use a RS232 transmitter between the two PLC's and exchange the data. I hope this helps |
1/25/2010 12:40 PM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already discussed in the thread with the subject Transmitting a signal wirelessly!. Best regards O_Moderator |
Follow us on