2/18/2010 7:34 AM | |
Joined: 3/18/2009 Last visit: 2/8/2022 Posts: 306 Rating: (94) |
The size of a DB cannot be "unlimited". Maximum being 64KB. (Some smaller CPUs have smaller limit) I don't think you can change the size of a DB in CPU run. You can create and delete DBs with SFCs like CREAT_DB and DEL_DB. A maximum buffer length FIFO block (in SCL) is givenhere.(you have to pay :( ) You can read this entry and at least have an idea on one of the possibilities of implementing the buffer. |
Follow us on