2/22/2010 9:05 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
In PCS7 7.1, I want to increase the user range for FC's, FB's and DB's in CFC under customize->settings for compilation/download. |
Last edited by: Oreca at: 2/22/2010 9:06 PMIf I could help you, you can use the RATE button. Thank you. |
|
2/22/2010 9:08 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
It seems that it is bedtime for me... I found another post where my question is explained... maybe someone could tell me additional info....sorry Updated question: Can I just change the range after blocks are already created by the system? Will the system update the number at the next compilation? |
Last edited by: Oreca at: 2/22/2010 9:15 PMLast edited by: Oreca at: 2/22/2010 9:15 PMIf I could help you, you can use the RATE button. Thank you. |
|
Follow us on