Industry Online Support
Technical Forum
3/28/2010 12:05 AM | |
Posts: 1 Rating: (0) |
Are there any functions available to shutdown the PCU when running Win95? I've seen threads discussing the shutdown feature when WinXP is the OS... |
4/5/2010 1:11 PM | |
Posts: 20 Rating: (1) |
As I know there no such facility given . So I did it in my own way , and it worked successfully in PCU50 with WinNT . Can you try this and check? Changes in PCU50 Copy "upsexit.exe" to the "F:\mmc2" directory ( upsexit.exe is attached)Add the following task configuration entry to "F:\mmc2\regie.ini" Task 10 = name : = upsexit,Timeout := 60000,preload = False Add an entry for task 10 to "F:\mmc2\language\re_uk.ini" as follows Task 10 = name = "upsexit" Add an entry to the file "F:\mmc2\keys.ini" as follows KEY50.0 = Task:=10 Changes in PLC : In OB100: L 0 T DB19.DBB10 In any running FC: A I 40.0 // UPS POWER FAILURE INPUT JCN CNT L 50 T DB19.DBB10 CNT: NOP 1 A I 40.0 = Q 52.0 // POWER FAILURE INDICATION Attachmentupsexit.zip (98 Downloads) |
Follow us on