4/30/2010 3:22 PM | |
Joined: 10/7/2005 Last visit: 8/6/2024 Posts: 3015 Rating: (1054)
|
Hello Fatso to tell you the truth, I'drather convinceyou to throw your 150U in the bin and upgrade it to an S7, thentell you that you can actually add an Ethernet card to it. Nonetheless, it is your call and here's what you can do as far as I'm concerned (did I mention that I'drather throw your 150U in the bin and upgrade it to an S7?): A CP 535 can be used in your 150U central rack (6ES5150-3SB81) in Slots 13-16 (aka Slots "107","115","123", "131",if you closejumpers 1-8 on the backplane of your CR you can also use Slots 18&19 (aka "147" &"155"). This is unfortunately as much advise as I can give you on this subject. I never attempted to add an Etehrnet CP to a 150U myself and most likely never will (and should a customer ask me to do so I'd tell him that I'drather throw his150U in the bin and upgrade it to an S7). There's also not too much documentation available on the Siemens web for it (and I had to look up the above info in the German manual which is available for download). I hope this helps anyhow and good luck |
Cheers |
|
Follow us on