5/18/2010 11:01 AM | |
Joined: 8/25/2006 Last visit: 8/15/2024 Posts: 2208 Rating:
|
When I say about setpoint channel I mean all channel where the setpoint may be, i.e. if you look to sheets G127-G135 (function diagrams in the manual) you will see how the setpoint is processing in the drive. For connecting the setpoint from DriveMonitor you may look here. If you use connector X300 (USS interface 1) for connecting your PC to the drive, you must set the following parameters to use speed setpoint from DriveMonitor: P433 or P484 or P438 or P443 or P644 = K2002 (2nd word from USS1, see sheet G170 in function diagrams). Also you may want to use ON/OFF command from DriveMonitor, so use B2100 as ON/OFF1 in control word (P654=B2100). |
5/18/2010 2:22 PM | |
Posts: 3 Rating:
|
thanks, that helped. I just had to change P051=40 in order to be able to apply those changes. |
Follow us on