Industry Online Support
Technical Forum
5/30/2010 4:15 PM | |
Posts: 2 Rating: (0) |
Bonsoir, Je suis en formaion S5/S7 et je dois faire un projet. Je me rapelle plus comment travaille le bloc fb avec le bloc fc Pouvez vous m'éclairer? |
5/30/2010 5:46 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
If I could understand you correctly, I think you need to know the differences between FC & FB. Her it is in this thread Regards, |
Ayman Elotaify |
|
5/30/2010 8:01 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello DEMEYER, This is international version of Siemens Automation forum. And we should use English language. In future just use this language. Hope you understand it. I'll try to translate your question.
Just if someone could add something more. Best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 5/30/2010 8:03 PMLast edited by: UMENCHO at: 5/30/2010 8:01 PM |
|
5/30/2010 9:40 PM | |
Joined: 9/27/2006 Last visit: 4/30/2024 Posts: 12257 Rating: (2666) |
Bonsoir, Demayer; Les réponses de ce forum seront données soit en anglais, soit en allemand. Par contre, les manuels et les liens suggérés peuvent être sélectionnés en français, si ça vous rend la vie plus facile; <Good evening, Demayer; Answers on this forum will be given in English or in German. However, suggested manuals and links can be downloaded in French, if this makes your life easier> Along with Step 7 program installation on your compueter, there were some programming manuals made available to you (in Simatic/Documentation). 2 will be of help in your situation: -Working with Step 7, First Steps (also foundhere: http://support.automation.siemens.com/WW/view/en/18652511) and -Programming with Step 7 (also found here: http://support.automation.siemens.com/WW/view/en/18652056) With these you should have good examples of how FCs and FBs interface, how they are called, and how to use them generally. Hope this helps, Daniel Chartiert |
5/30/2010 11:02 PM | |
Posts: 2 Rating: (0) |
merci je ferais un effort |
5/31/2010 5:57 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
|
Follow us on