5/24/2010 11:35 AM | |
Posts: 7 Rating: (0) |
Dear All, I was checking in the manual of Simocode PRO section earth fault monitoring (attached). For Internal earth fault function, there issuch note : Quote --- The normal operating condition up to 2 x Is. The effective Operating Current must be smaller than twice the Set Current Is. Fault Currents of > 30% of the Set Current Is will be detected AttachmentManual Simocode Pro V_060307_earth fault monitoring.pdf (405 Downloads) |
Follow us on