8/31/2006 3:31 PM | |
Posts: 8 Rating: (0) |
Dear sir, In 802D manuals I found LIMS is also active in G97 which seems to be in line with your findings. But it should be possible to program LIMS in one line with G97, ie. G97 LIMS=3500 S3500 With regards to the machinedatum, the parameter for 35500 is already set at '1' for all axis and 35150 is set at "0.10" for all axis. MD 35500 only works when there is a measured speed value from the spindle available, ie a spindle encoder. Otherwise MD35500 takes the programmedspeed as the actual speed and basically there is no monitoring. Also realize that setting MD35150 to 0,1 means that the actual speed may differ by 10% before feedmove can start, so with a programmed speed of 3000, the tool starts cutting at 2700 already. In case of questions, you can always try to use our support-request website: |
Follow us on