6/11/2010 12:31 AM | |
Posts: 2 Rating:
|
hello could someone explain why "monitor from callup path" is only an option on on some multiple instance FBs in my programme. the FBs were only "monitor" is an option makes it difficult to interogate specific instances Examlpe Motor 1 = FB50 can montitor from call path Motor 2 = FB50 only monitor CPU =317DP/PN Thanks if you could help Splitted from Help S7 300 315. |
Last edited by: O_Moderator at: 6/11/2010 2:02 PMnew subject after splitting |
|
6/11/2010 11:27 PM | |
Joined: 10/7/2005 Last visit: 6/24/2024 Posts: 3008 Rating:
|
Hello dh5306 I'm afraid I can't answer that, as it should work for all calls in the same way. I do wonder though if you open the online version of your Block ("Monitor with call up path" is not yet the most intuitive function to use). Have a look atTHIS desciption for more andplease let us know if it fixes your problem. |
Cheers |
|
This contribution was helpful to
1 thankful Users |
Follow us on