3/10/2010 8:24 AM | |
Joined: 4/5/2006 Last visit: 4/24/2024 Posts: 917 Rating: (63) |
Hi Mohebbi, did you already seen previuos tread PCS7 F-Systems Download Error hope can help regards |
5/12/2010 8:32 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928) |
Is this problem solved?? I have a similar error code... |
If I could help you, you can use the RATE button. Thank you. |
|
5/13/2010 1:29 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928) |
Well, My problem is solved, i think.... Please check my post, maybe it helps you------>/tf/WW/en/Posts/43470#top The "virus" I had was removed, after that I got a back up project and now everything seems fine. Maybe the virus corrupted my project or Maybe I executed a wrong action-> compile SCL and directly downloaded it to program with inconsistency as conclusion. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on