5/31/2010 1:56 PM | |
Posts: 3609 Rating: (29) |
Import of a Technical Question of an User boopathi@sequent wrote: Dear All , wincc7.0 how to configure user login details in events.help me. send sample pdl (program) |
6/1/2010 7:40 AM | |
Posts: 63 Rating: (39) |
Dear Bhoopati, i will give u an example to create a ueser login on buttons click event First create a button and create a click event on it then go to the miscellaneous properties of it in that double click on Authorization and Click on user administration with the help of which u can only see the other dynamic properties like colour change etc. but not able to click on it untill u login via a user administration See enclosed for more information From Mack123 AttachmentUser Login.zip (245 Downloads) |
6/6/2010 2:29 PM |
|
Posts: 1 Rating: (0) |
|
6/26/2010 7:03 PM | |
Posts: 2661 Rating: (279)
|
Hi, See the following FAQ: How can you generate user-defined operator input messages in WinCC? |
Follow us on