Industry Online Support
Technical Forum
7/2/2010 9:14 AM | |
Joined: 4/24/2006 Last visit: 5/17/2024 Posts: 8649 Rating: (1151)
|
Dear lord.magnetica, If I understand it wright You want to set bit 1.1 when pressing some button on screen. You want to wait until Bit 1.2 is high. (Perhaps you can reset bit 1.1 in CPU, when Bit 1.2 is high) It is even possible to change screen by PLC, when bit 1.2 is high. You can use PLCjob to change screen or by changing a tag. (In WinCC flexible go to Tag managment and select the tag, go to properties and events -> Change value then select a function called Select screen or Select screen by number) how can you make a screen selection on a windows-based operator panel via the controller without using a controller job? Best regards, Wizard |
Last edited by: Wizard at: 7/2/2010 9:19 AMlink added |
|
Follow us on