6/29/2010 8:48 AM | |
Joined: 5/18/2010 Last visit: 8/18/2023 Posts: 24 Rating: (0) |
Hai all... I got a problem regarding the response time whenever i doing/change picture..The data too slow to process/update if any changes occur..I already set my i/o field and page to 250ms..But it won't work..What should i do..?i have no idea anymore to make my project smooth without lack of response time..I used PLC S5 135U and connect to WinCC 7.0.. Splitted from WinCC 7 project works very slow. |
Last edited by: O_Moderator at: 6/29/2010 10:42 AMnew subject after splitting |
|
7/8/2010 5:09 AM | |
Joined: 5/18/2010 Last visit: 8/18/2023 Posts: 24 Rating: (0) |
tq..i will follow all the direction...i will give feedback if anything... |
Follow us on