Industry Online Support
Technical Forum
7/26/2010 11:27 AM | |
Posts: 2964 Rating: (481) |
Hello... Does your motor encoder is also absolute? what type of 611D card is used? the parameter values what you havemadeevery thing seems to be OK. could you also check this parameter too... 1) 30230[1] Encoder input NR= 2 (*if A axis encoder is connected on 611D card X421 port) 2)30280[1] ENC_ASSIGN_ACTIVE_DRIVE[1,AX1]=0 Since it is connected on same 611D card no need to mention machine axis number. 3)34200[0] and [1] ENC_REFP_MODE=0 4)1007 ENC_RESOL_DIRECT= ( Marks /rev) for your reference i am attaching Absolute measuring system settings (EnDat interface). check it out... AttachmentLinear_Abs_Meas_Config.pdf (206 Downloads) |
This contribution was helpful to1 thankful Users |
7/27/2010 8:15 PM | |
Posts: 19 Rating: (0) |
we are using an external encoder which absolute Endat (13 bit) which is connected with a gear ratio of 1: 2.5 |
Follow us on