Industry Online Support
Technical Forum
8/20/2010 6:15 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello GaryMc, 6RA2281 = 400 Amp DC converter is OK. But what about 69v62-0. Pls check up & confirm this. Also it is not clear whether this is 1Q or 4Q drive. You have specified as drive has analog signal on terminal 12 & 13, but not specified on which card. On A1 card terminal 12 & 13 are out put analogue signals of +/- 10V for actual current value. You have not specified about terminals 11 & 15, are of which cards. Please find attached here with 6RA22 drive data sheets. You can refer these so that you can have idea about drive technical data, position &locations of different cards & ribben cables in the drive & drive connection block diagram. Hope this shall help you. Regards, DEEP. Attachment6RA22 drive data.pdf (194 Downloads) |
Last edited by: DEEPSTR2010 at: 8/20/2010 6:46 AMAttached attachement |
|
Follow us on