Industry Online Support
Technical Forum
8/23/2010 2:31 PM | |
Posts: 159 Rating: (3) |
Hello! I have a PCS 7 v7.0 Sp3 with ES, one OSClient and one OSServer setup. I have some problems with the SFB35 (Alarm_8p) block in my CFC. I have configured the block as opposed in the documentation (had not this problem when my system were running as singlestation). After compile\download, when the "SIG_1" on the Alarm_8P i true, the alarm shows in WinCC. So far so good But my problem is that the Message text is missing in WinCC!, eventhough I have configured it in CFC!(see picture) Could this be because of my "Standard server" settings in the client? (see submitted picture) I must admit that I dont have full understanding of the standard settings... AttachmentMessage text.zip (110 Downloads) |
9/10/2010 2:55 PM | |
Posts: 159 Rating: (3) |
Runis, Thank you very much for your reply. Tride what you suggested and it worked. |
Follow us on