9/8/2010 7:32 PM | |
Joined: 2/1/2010 Last visit: 5/29/2024 Posts: 144 Rating: (70) |
Is it possible to use the USB PC Adapter 6es7 972-0cb20-0xa0 as a standard RS-485/Modbus connection com port? Since Profibus DP is a subset of RS-485 this should be possible technically, but maybe drivers don't support this? I'm stuck on location without my other RS-485 adapter and need to change Modbus slave addresses via a 3rd party software tool on devices connected toa CP341 Modbus RTU Master. Thanks for any advice. |
If my post helped you, please rate. Thanks. |
|
Follow us on