9/18/2010 6:56 PM | |
Posts: 32 Rating: (0) |
Hi, I have an application with WinCC V7.0, a PLC S7-314 with CP343-1Lean and a Sentron PAC3200. Is possible to connect the PC, PLC and PAC3200 in a ethernet network using Modbus TCP protocol? What do I need to do for this one? If somebody can help me with an example. Splitted from Modbus TCP/IP in WINCC V7.0. |
Last edited by: O_Moderator at: 9/20/2010 12:50 PMnew subject after splitting |
|
9/20/2010 12:06 PM | |
Joined: 1/4/2010 Last visit: 5/2/2024 Posts: 650 Rating: (40)
|
Hi Please have a look in this docu: https://www.automation.siemens.com/mdm/default.aspx?DocVersionId=16484411147&TopicId=12178878603 Also there are some Threats in forum about Modbus perhaps they helps: /tf/WW/en/Posts/48565 /tf/WW/en/Posts/48627 or please search again in the forum. |
Regards |
|
9/20/2010 12:51 PM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already discussed in the following thread Wincc modbus tcp . Best regards O_Moderator |
Follow us on