Industry Online Support
Technical Forum
9/26/2010 11:59 AM | |
Posts: 325 Rating: (13) |
Hi, Got a new PCS7 s/w V7.1 SP1. Things go well till Simatic Manager. I am able to compile CFC and OS. Got problem with Wincc Runtime. The moment Wincc(V7.1 SP1 HF4) is opened, we are able to view all the tags which got compiled during OS compilation. When wincc goes into runtime, none of the buttons work and no picture appears. Even the picture tree navigator is disabled. Had a look at the following post, but that didn't help me.... /tf/WW/en/Posts/39784 Regards Nil |
9/26/2010 3:16 PM | |
Joined: 11/15/2009 Last visit: 2/5/2024 Posts: 380 Rating: (47) |
Hello Nil96 Execute “Simatic Security Conrtols” can help you. Regards |
Follow us on