Industry Online Support
Technical Forum
9/24/2010 3:45 PM | |
Joined: 9/27/2006 Last visit: 6/16/2024 Posts: 12260 Rating: (2671) |
Hello Tuff Gong; The following information is extracted from the Simatic WinCC Brocure (2009): https://www.automation.siemens.com/salesmaterial-as/brochure/en/brochure_simatic-wincc_en.pdf?HTTPS=REDIR Number of connectable controllers For communication via Industrial Ethernet with a CP 1613 communications processor, with a maximum message frame length of 512 bytes up to 60 SIMATIC S5/505 Controllers or upto 64 SIMATIC S7 Controllers and via PROFIBUS with a CP 5613 a max. of 44 controllers (CP 5611 max. 8) can be connected. With approx. 10 or more controllers, the use of Industrial Ethernet is recommended.
WinCC system software The WinCC system software is available in two basic variants: • WinCC complete package (RC: license for runtime and configuring) • WinCC runtime package (RT: runtime license) Both packages are available with 128, 512, 2k, 8k, 64k, 100k, 150k or 256k PowerTags. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 9/24/2010 3:47 PM |
|
9/24/2010 5:54 PM | |
Posts: 41 Rating: (1) |
It does. Thanks |
Follow us on