10/18/2010 5:17 PM | |
Posts: 116 Rating: (7) |
Hi, which ordering number of D435 ????? Do you see anything in the diagnostic buffer ? Regard Jerry |
10/19/2010 8:22 AM | |
Posts: 116 Rating: (7) |
Hi, it could be that there is an aditional HW restriction for the BIOS update -- I try to find it out. Regards Jerry |
10/19/2010 2:34 PM | |
Posts: 116 Rating: (7) |
Hi, what is sure is that "< C" won't work. >> I have also tried this on a HW version "C" << --> sure that it won't work? What BIOS Version is shown and what shows the diagnostic buffer? Regards Jerry |
This contribution was helpful to1 thankful Users |
10/19/2010 2:44 PM | |
Posts: 31 Rating: (0) |
Jerry, You are correct, it seems my "C" version did work. The Bios version is now 02.02.00.00, and the diagnostic buffer says "Status 3" at the end of it. Thanks for you help. In my opinion the restrictions need to be better stated in the manual (as well as the procedure) |
10/19/2010 9:37 PM | |
Posts: 116 Rating: (7) |
Hi, now everything is how it should be (...besides the description in the manual....) You can be sure, that this will be changed with the next version of the manual. Regards Jerry |
Follow us on