Industry Online Support
Technical Forum
10/21/2010 2:24 PM | |
Posts: 96 Rating: (10) |
HI mhaiz1, From you post it seems like the system is running and you can see the trends in the runtimeenvironment. If you can see the trends then you should see them in the process object view (archivetab), as long as they are done automatically the PCS7 and notmanuallyinserted in the WinCC tag logging. Make sure you are selecting thehierarchylevel. Other wise you can do whatJOTSTsaidile>Print Project Dokumentation in WinCC tag logging. I also export the list from the WinCC Tag logging just in case if some one has inserted tag manually. Hope this was helpful. Regards, |
10/21/2010 3:38 PM | |
Posts: 5 Rating: (0) |
I believe that answers my question. They must have been created manually. |
Follow us on