Industry Online Support
Technical Forum
11/1/2010 1:43 PM | |
Posts: 8 Rating: (0) |
Thanks perdahlqvist, Works for me. regards CTTEP |
11/2/2010 7:24 AM | |
Joined: 1/17/2006 Last visit: 5/29/2024 Posts: 800 Rating: (63) |
Hi, be carefull with char String="text"; it's a memory leak if you do not use sysaloc. |
11/2/2010 9:24 AM | |
Posts: 8 Rating: (0) |
Hello Japie, Thanks for the advise. char String="text"; is not quit the way I use it. I had problems isolating one specific character in a text. What I am doing is garding a specific IP adres, based on a ping command that is redirected to file. Such a file is always made up the same and contains on line 10 always the number of packets lost. That number is the character I want to isolate and do something with. The algorithm that I use is based on the test script in the uploaded text file. Mind you the coment is in Dutch, but your nickname on this forem sounds Dutch to, so maybe that's no problem. Regards CTTEP AttachmentScript.zip (100 Downloads) |
Follow us on