Industry Online Support
Technical Forum
11/5/2010 8:32 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (308) |
Hello, All ports of the X108 switch have the same working, and they do not assume any special role in server switchover. Software in the servers decide about that. A possible option is S7-redconnect. The AS400-H may is in most cases equipped two communication processors CP443-1. Each server can setup one or two S7 connections (one to each CP443-1). |
Best regards |
|
Follow us on