11/29/2010 6:54 PM | |
Joined: 3/7/2006 Last visit: 8/6/2024 Posts: 37 Rating: (2) |
I programmed it with no scripts, all direct connection. I work with a dword and then I extract with a vbs script all the bits I need to connect the status display tags. I post my old faceplate type and the new one. You will see that the only difference is the graphic objects instead of status displays. I've won 14 seconds in a picture with aprox 50 objects (valves, motors, analogs, PID and others). Here we go... Thank you in advance. AttachmentFaceplate_Type.zip (98 Downloads) |
Follow us on