10/25/2006 8:57 AM | |
Joined: 4/24/2006 Last visit: 4/22/2024 Posts: 8611 Rating: (1147) |
Hi, |
10/25/2006 4:45 PM | |
Joined: 4/24/2006 Last visit: 4/22/2024 Posts: 8611 Rating: (1147) |
Hi, Perhaps in the control panel of windows, you can find Setting PG/PC interface? Best regards, Wizard |
10/26/2006 1:18 PM | |
Joined: 4/24/2006 Last visit: 4/22/2024 Posts: 8611 Rating: (1147) |
Hello, Did you already install Hotfix 5? You can download from here: http://support.automation.siemens.com/WW/view/en/24104401 Unfortunately I don't have the chance to test something with S7-200. When I do a test with S7-300, everything is working as expected. There is a connection between S7-300 and simulation of MP, tags are being updated. Best regards, Wizard |
Follow us on