Industry Online Support
Technical Forum
1/11/2011 9:29 AM | |
Posts: 90 Rating: (1) |
Hello people! I have a PC-WinCC flexible runtime connected to Internet. I want to remotely control the PC-SCADA from a PC connected to Internet through Internet Explorer. What option do I need: Sm@rtAccess or Sm@rtService? Thank you in advance. Kind regards, Beep |
1/11/2011 9:53 AM | |
Joined: 4/29/2010 Last visit: 8/12/2024 Posts: 1557 Rating: (161)
|
Hello, both options supports this function. If you just want to remotly control this device via IE then Sm@rtService is the right one. Check also this manual, there are these two options are explained: WinCC flexible Options This faq can also be helpfull for you i think: What are the options for remote maintenance of a WinCC flexible Runtime system (Panel/PC) via the Internet (WAN)? best reagards. |
1/12/2011 8:14 AM | |
Posts: 90 Rating: (1) |
Hello Sandman Thank you for the useful informations. Kind regards, Beep |
Follow us on