2/11/2011 9:49 AM | |
Posts: 63 Rating: (0) |
Hi members, I tried the First step program "FAST" of PCS7, at the and i got a problem. When i compiled and download the program i got that massage:Error occurred compiling the object If i conitune the program i can't simulate the OS(1). Please see the attachment. Best regard. AttachmentCompile and Download Objects.pdf (49 Downloads) |
2/11/2011 10:01 AM | |
Posts: 63 Rating: (0) |
Thanks a lot zerepegro I did it and added the file. Regards, Fatih AttachmentTRANSFER.pdf (52 Downloads) |
2/11/2011 12:59 PM | |
Posts: 63 Rating: (0) |
Hallo zerepegro, Thanks for your reply, How can i learn the DM variables numbers in VinCC which i use them with license. Regards. |
2/18/2011 4:51 PM | |
Posts: 63 Rating: (0) |
Hi zerepegro, AttachmentTRANSFER.pdf (101 Downloads) |
2/23/2011 1:36 PM | |
Posts: 183 Rating: (8) |
Hello f.arslan; If the POs are not already transferredyou need a RC license to transfer the POs to the OS.Then you will be able to simulate the OS with PLCSim. |
Follow us on