3/7/2011 7:14 PM | |
Posts: 14 Rating:
|
Hi How can I perform memory reset of CPU 414H.Is it performed from key switched or by STEP7.Operating system can request and do memory reset? Thank you |
3/8/2011 9:32 AM | |
Joined: 7/2/2008 Last visit: 5/29/2024 Posts: 928 Rating:
|
Dear lidumazie,
A memory reset meansclearing RAM. You can use the MRES switch to reset the CPU and you can do it as well through STEP7. You can read the following in In S7-400H manual
If you would like to do it in SIMATIC Manager, all you have to do is to select the PLC>Diagnostic/setting>Clear/reset. Both methods will not erase the contents of an EPROM and if you were asking how to erase or clear an EPROM, you have to put your flash card in a programming device(SIMATIC PG)and in SIMATIC Managergo File>S7 memory card>delete. Best regards. H-H |
This contribution was helpful to
6 thankful Users |
3/8/2011 7:36 PM | |
Posts: 14 Rating:
|
Thank you H-H Inserting a EEROM to the CPU may cause a memory reset in CPU? THANKS |
Follow us on