3/14/2011 2:57 PM | |
Posts: 8 Rating:
|
Hello, I've Windows VISTA 64 bits, so I tryed to use the software TIA - STEP 7 10.5 on a virtual machine (windows xp 32 bits). The software was installed with no problems, but the PC doesn't connect with the PLC S7-1200. I tryed configure the virtual machine network with NAT and Bridge, but the problem is the same, in both cases. My virtual machine is the VirtualBox, there is a problem between this VM and the STEP 7? There one more step, to do, when is used virtual machine? Thanks Bruno Splitted from Simatic S7-1200 on Vista 64 or Windows7 64. Splitted from |
Last edited by: O_Moderator at: 3/15/2011 10:41 AMnew subject after splitting |
|
Follow us on