Industry Online Support
Technical Forum
3/28/2011 2:48 PM | |
Posts: 46 Rating: (0) |
I am currently using NVDIA graphic card for Dual monitor in one PC. By using OS project editor i can display graphics in both monitors. The problem is all the clicked button of graphic switching only happen in primary monitor, even pop up screen also only show in primary monitor only. So may i know what is the problem? Is there any script needed? Please help as currently need to solve this problem asap. Thanks for the help. Splitted from Two or three monitors in one pc. |
Last edited by: O_Moderator at: 3/29/2011 9:42 AMlink edited Last edited by: O_Moderator at: 3/29/2011 9:42 AMnew subject after splitting |
|
3/29/2011 9:43 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already published in the following thread duo monitors display. Best regards O_Moderator |
Follow us on