Industry Online Support
Technical Forum
3/20/2011 9:02 PM | |
Posts: 9 Rating: (0) |
Hy I have sistem with PLC S7 CPU 312; 6ES7 307-1EA00-0AB0, and I programing with STEP 7 Lite. I initially built the system with pneumatic cylinders and motors, with whom I have managed over the PLC, and all functioned normally, and I programmed. Since the system looks statically unstable so I had to redesign the cylinder carriers and create a new cabinet plc. When I finished and then started connecting PLC with inputs and outputs, I tried to make a small program to test the inputs and outputs. Then Plc reported an error. Program and hardware configurations were successfully transferred to the PLC, but when I try to run the program to the PLC, the LEDs reported an error. SF LED is on 5VDC is. on STOP is. on I tried to dowload OB55, OB56, OB57, but it is not possible. Everything else is possible to download the PLC unless stated OBS Attached is: Module information with mistake Online CPU and Hardware I do not understand: Event 1 of 107: Event ID 16 # 49A4 CAN SOMEONE HELP ME, WHAT SHOULD I DO TO RESET ERROR AttachmentModule Information.pdf (123 Downloads) |
Follow us on