11/26/2009 8:26 PM | |
Joined: 10/30/2008 Last visit: 5/15/2024 Posts: 64 Rating: (2) |
Good Fun! |
Tiago Martins Machado |
|
11/30/2009 3:13 PM | |
Posts: 3 Rating: (0) |
Thx Robster, It sounds like a load of fun! I guess this product is still very immature. Either that or they want us to keep using the S7-200. Khek |
12/18/2009 9:29 PM | |
Joined: 9/23/2005 Last visit: 6/17/2024 Posts: 4346 Rating: (1434)
|
Hi, With SP2 of STEP7 Basic (http://support.automation.siemens.com/BR/view/en/39741113 ) it is possible to access single elements indirectly in an array (news instructions: FieldRead and FieldWrite). This could be used (not 100% easy) to implement FIFO functions. |
Denilson Pegaia |
|
12/21/2009 1:21 PM | |
Posts: 3 Rating: (0) |
Thanx Pegaia! I'm ready to go back to V10 and do everything in STL! |
5/1/2011 7:44 PM | |
Posts: 15 Rating: (0) |
Hello khekd I've made a block for buffering data in the S7-1200. Please have a look at this entry in the forum. It might be helpful to you perhaps. Please note, this is provided to assist you and I / my company can not claim any responsibility even though the block has had rigorous tests. Hope this helps. Best regards, Rohit Bhatia |
Follow us on