5/15/2011 12:17 PM | |
Joined: 10/7/2005 Last visit: 9/5/2024 Posts: 3018 Rating:
|
Hello S_W_11 it's impossible to say when "AT 70" will give you an RLO of 1 asit all depends on the type of Timer used (e.g. if T70 is started as an On delay Timer, it will give you a RLO of 1 when the time has expired, if T70 is started as an Off delay Timerit will give you a RLO of 1 as soon as the Timer start condition becomes trueetc.). I suggest you do the following: Right click T70, select "Go To Location",go to the locationin the program where the T70 is started and use <F1> to get the context sensitive help on it. I hope this helps |
Cheers |
|
Follow us on