5/21/2011 9:49 AM | |
Posts: 8946 Rating: (999) |
It is true. It make no sense anymore to design new plants with S7-200. |
5/21/2011 10:18 AM | |
Joined: 5/28/2008 Last visit: 10/7/2024 Posts: 4515 Rating: (839)
|
Hello, There is no official announcement that S7-200 will enter product discontinuation phase soon. There is no official announcemoent that S7-1200 is the successor of S7-200. There are some clients still need and prefer using S7-200 due to Prices. Although S7-1200 have more features. The best place tknow if S7-200 willenter product discontinuation phase is Siemens web site. Write the part number of S7-200 module in the search and open the product page and see the product life cycle for each module. Here's in this link an example ofCPU224XPproduct life cycle. Hope this helps. |
Ayman Elotaify |
|
5/22/2011 9:26 AM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
|
Ammy |
|
Follow us on