4/28/2011 6:50 AM | |
Joined: 3/21/2006 Last visit: 11/1/2024 Posts: 10229 Rating: (1181) |
Hello, According to the its update announce seems is correct.
But this error means something wrong in configuration. For more look there - SYSTEM DATA PROBLEM IN CPU-313C Did you receive any error durring Save&Compile? Best regards, Hristo Mihalev |
4/28/2011 8:18 AM | |
Joined: 3/23/2010 Last visit: 11/11/2024 Posts: 20 Rating: (0) |
Hello Hristo Mihalev, you have right, I just take notice that I receive error message during compile. (the system data could not be recreated because the configuration is inconsistent). I had writed , I settle cp 343-1 Lean v 2.0 to slot 10 instead of cp 343-1 Lean v 2.3 . because there is no cp 343-1 Lean v2.3 in catalog. here my project. by the way, I couldn't add that cp 343 to hardware, please you add cp 343 v 2.3 to hardware. or please give me idea. waiting your replay I m sending my best regards. AttachmentZimp_fil.zip (157 Downloads) |
4/28/2011 8:55 AM | |
Posts: 691 Rating: (37) |
Hey crazy I got your solution See the attached pic You forgot to assign the network |
4/28/2011 9:04 AM | |
Posts: 316 Rating: (37) |
Hi crazy, I think you can update your CP to FW V 2.3, butcan'tconfiguratethe V 2.3 in HW config.But the engineeredV 2.0 should works with realV 2.3. http://support.automation.siemens.com/WW/view/en/42122470 For the other problem make the following: - clear the system data on your plc - donwload the HW config again. Then it should work, I think. |
Follow us on