5/25/2011 10:42 AM |
|
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating: (86) |
Hi What EFKA has said is right, It is simple to use user administrator, and select the are you want. Have fun... |
Jazz |
|
5/25/2011 11:09 AM | |
Posts: 13 Rating: (0) |
Thank you guys. Have tried a lot of that stuff earlier, but tried playing around a bit more with it now. Still can't get it to work. Please see attached pdf with a more detailed description of my problem. I have also tried creating my own button and not using the areabuttons in @areabuttons.pdl, then it actually works as it's supposed to, but by doing that I get some problems with for instance setting the backcolor when the picture is selected due to using several screens. If you could take a look at the pdf and come back with some more tips I would really appreciate it. AttachmentAreabuttons.pdf (198 Downloads) |
5/25/2011 11:45 AM | |
Posts: 799 Rating: (43)
|
Hello again, now I tried on my site in little test project and it works. I don't know, what is wrong in your project, because on the first look, the screenshots seem to be ok. Maybe your user administrator was already opened before you executed the OS Project editor. Is that possible? I tried also with normal buttons, "outside" of the basic process control (OS Project Editor), and this also works. Maybe you should also take a look into the WinCC Information System. There's a chapter called "Structure of the User Administration". I think this can be also very useful to you. So far best regards |
5/27/2011 5:01 PM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating: (86) |
Hi Nice to hear that it is working. Good work... Have fun,... |
Jazz |
|
Follow us on