5/30/2011 10:32 AM | |
Posts: 291 Rating: (69) |
Hi paramo123, I know you must be feeling very confused about the "kinds" of SmartTags. Would you please take a look at the faceplate attached? Then you should be able to know what I was talking. Good luck, Komi P.S.: This one doesn't mean the FP can be ran without error totally in Web browser. It can be shown correctly. But ...due to the problem of taking use of SmartTags("InternalVariable"), I found it will be in vain if I want to set/ modify value back to the linked External HMIRuntime Tags. *** Everything's working fine in WinCC Runtime Station/ Base System. Any modifcation of value done in the FP, will be applied/ written back tolinked External HMIRuntime Tags. AttachmentKomiFp_16Bit_Rev1.zip (202 Downloads) |
5/30/2011 11:23 AM | |
Posts: 9 Rating: (0) |
Hi Komi, Please refer to our FPT Screen. AttachmentFPT Screen.zip (225 Downloads) |
5/30/2011 11:51 AM | |
Posts: 291 Rating: (69) |
Hi pramo123, Thanks for uploading yours. Surely I'll try it tomorrow. & will tell you the result. B.R., Komi |
5/30/2011 7:30 PM | |
Posts: 291 Rating: (69) |
Hello Pramo123, Congratulations to both you & me! I've modified your .ftp & tested it in the WebNavigator and found "almost everything" is running fine. Don't worry ~ You had two small syntax error only: Err1 is at the TooltipText_Trigger of the property event of your Group object. Err2 is at the vstate_event: OutputValueChange ~ you wrote "ScreenItem" in somewhere where should be "SmartTags" ;-) Besides, I said "almost everything" ~ because somewhere you're using "user_cycle" for screen(appearance) _updating ...The flashing effect won't be felt due to this updating cycle set! Anyway ~ Please refer to the attachment. & take the modified ftp please! B.R., Komi
AttachmentTYP_MOTOR_K.zip (201 Downloads) |
5/30/2011 7:56 PM | |
Posts: 291 Rating: (69) |
I faild to upload the video file for more than 10 times. Hoping this time will get through ~ but pity... I will try upload by another way later on! BTW, I need to appologize for that ...my previous test failed in taking use of SmartTags was because I hadn't disabled the Authorization No. 1002 (WebNavigator Client--Monitoring only). I was too carefulness & too stupid. (Actually ~ I saw the "!" mark with "no input" alert...*-*;) Well ~ so now I know it's totally okay for Faceplate being displayed & controlled in WebNavigater. Sorry again! Komi
AttachmentP123_Movie.zip (195 Downloads) |
Last edited by: Komi at: 5/31/2011 3:29 AM |
|
5/31/2011 7:29 AM | |
Joined: 10/3/2010 Last visit: 10/31/2024 Posts: 1563 Rating: (192) |
Komi, you're doing such a great job on here. You really should create your own demo project for us |
B r g d s , |
|
This contribution was helpful to1 thankful Users |
5/31/2011 9:06 AM | |
Posts: 9 Rating: (0) |
Hi Komi, Thanks for your effort.I changed my script instead of smarttags,screenitems is used.Now it is working fine By Pramo123 |
Follow us on