Industry Online Support
Technical Forum
6/2/2011 2:38 PM | |
Joined: 7/2/2008 Last visit: 4/5/2024 Posts: 928 Rating: (305) |
Hello Nil,
I'm sorry but it's not possible to have hot swapping with software redundancy based on S7-300 CPU. Even with the GSD file it is still not possible.
Unfortunately the only switchable IM153 is the IM153-2 HF. That's the one used with either software redundancy or H-system. So, the IM153-4 (i.e Profinet solution) will not work. Best regards. H-H |
This contribution was helpful to1 thankful Users |
Follow us on