12/4/2006 9:34 AM | |
Posts: 1776 Rating:
|
Hi, have a look a the following link chapter 1 Also have a look at the FAQ |
12/4/2006 10:15 AM | |
Posts: 5822 Rating:
|
Hello, I can tell you that it is no deal to use any other Switch you want instead of the ASGE Star coupler, as long as you do not use the SNMP with it, if you use the SNMP functions of the ASGE Star coupler you will have to change a bit of your configuration but that’s it. The CP1430 you mentioned does not need the AUI RJ45 Transceiver you talked about earlier. The CP requires a special cable that switches the Interface from AUI to ITP which is signal compatible with RJ45. This cable is mentioned in the Catalogue IK PI 2007. I add to this Post a short extraction of an older version of the IK PI for you to see. Best regards J_Bell AttachmentRJ45_-_15_pin_Cable_76.pdf (373 Downloads) |
Follow us on