Industry Online Support
Technical Forum
6/9/2011 7:07 AM | |
Posts: 291 Rating: (69) |
Hi lalu, Would you please test this first ? https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=43101218&caller=view Do you have an existing WPF Trend Control created by yourself ? or Do you mean that you need one & need to know the usage as well? Regards, Komi |
6/15/2011 9:24 AM | |
Posts: 38 Rating: (0) |
Hello, I have used Calculator and it works fine.I need WPF Trend Control to use in WinCC. Regards Manish |
6/15/2011 9:37 AM | |
Joined: 10/3/2010 Last visit: 9/20/2024 Posts: 1562 Rating: (191) |
Maybe check Visifire [code]Visifire is a set of data visualization controls - powered by Microsoft Silverlight & WPF. Visifire is a multi-targeting control which can be used in both WPF & Silverlight applications. Use the same API to create charts & gauges in Mobile, Web & Desktop environments. Visifire Silverlight Controls can also be embedded in any webpage as a standalone Silverlight App. Visifire is independent of server side technology. It can be used with ASP, ASP.Net, SharePoint, PHP, JSP, ColdFusion, Python, Ruby or just simple HTML. Don't take our word for it! Visit Visifire Gallery or design your own chart or gauge using Chart/Gauge Designer.[/code] http://www.visifire.com/ |
Last edited by: SteBo at: 6/15/2011 9:37 AMB r g d s , |
|
Follow us on