5/25/2011 11:48 AM | |
Joined: 10/3/2010 Last visit: 7/31/2024 Posts: 1560 Rating:
|
Or install one of them in a virtual machine |
B r g d s , |
|
6/16/2011 5:43 PM | |
Joined: 8/31/2010 Last visit: 8/5/2024 Posts: 1519 Rating:
|
Hi KalaDGT, I am also facing the same problem. As of now WinCC Professional v11 cannot be installed on a PC where WinCC v7.0 SP2 is already installed. Side by side installation of WinCC Basic / Comfort / Advanced and WinCC v7.0 SP2 is only possible. Refer the Compatibility with other SIMATIC products ->Side-by-side installation with SIMATIC products SIMATIC WinCC v11 Soon there should be some way for the parallel installaion of WinCC Professional v11 and WinCC v7. |
Like it? Rate it! |
|
This contribution was helpful to
1 thankful Users |
Follow us on