Industry Online Support
Technical Forum
5/29/2011 8:08 AM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359) |
Dear members I found the following links useful to undrestand the basic operation of PID controller. PID control and associated controller types 1-The classical three-term PID controller 2-Optimal tuning of PID controllers 3-Advantages and disadvantages of the different types of controllers 4-Empirical tuning rules according to Ziegler and Nichols Also, check here for more control topics: http://www.atp.ruhr-uni-bochum.de/rt1/syscontrol/node1.html Regards |
This contribution was helpful to1 thankful Users |
5/29/2011 8:38 AM | |
Posts: 8946 Rating: (999) |
Better way, buy this book: http://www.amazon.de/Controlling-SIMATIC-Practice-Control-Systems/dp/3895782556 |
5/29/2011 8:50 AM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359) |
Yes, The book is the best refernce while working with SIMATIC family.The infornation provided here if free of charge and as I remember section 1-2-2 and 1-2-3 of the mentioned BOOK cover the same material. Also the new version in German will be on market in July 2011. Regeln mit SIMATIC (Juli 2011) Regards |
7/20/2011 11:51 PM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359) |
[quote ] Also the new version in German will be on market in July 2011. Regeln mit SIMATIC (Juli 2011) [/quote ] Releasing the new German version of the book postponed till August 2011.This is the 3rd time as I remember.The book is in the pipeline till then. Regeln mit SIMATIC (August 2011) Regards |
Last edited by: hdhosseini at: 7/21/2011 8:57 PMLast edited by: hdhosseini at: 7/20/2011 11:59 PM |
|
Follow us on