12/19/2006 12:16 PM | |
Posts: 1 Rating: (0) |
Hello, Currently i'm working with a PCS7 system, with CPU417-4H and i need to prepare communications with a ComBox-P (which is a protocol converter from modbus to profibus)as profibus slave ; the ComBox-P is being use by ATLAS COPCO for managing a Can Bus. I have received the GSD as well as a general manual with a brief explanation about how it works, but it doesn't explain anything about the configuration of the GSDwhen using as a DP slave. AttachmentProfiCan.zip (2196 Downloads) |
This contribution was helpful to2 thankful Users |
Follow us on