Industry Online Support
Technical Forum
8/16/2011 12:28 AM | |
Posts: 48 Rating: (1) |
Dear BEVEE, THANK YOU FOR YOUR REPLY. I HAVE PG 730 PROGRAMER WHICH WORKS UNDER DOS , SO I HAVE TO SETUP THE COMGRAPH PROGRAM, WHER I CAN FIND THIS PROGRAM AND HOW I CAN SETUP ON THE PG 730? WAITING YOU THANKS Splitted from i have monitor with R-G-P cables connected to communication processor(6AV1242-0AB10) in S5 135U with CPU 928B. |
Last edited by: O_Moderator at: 8/16/2011 10:57 AMnew subject after splitting |
|
8/16/2011 10:57 AM | |
Joined: 4/24/2009 Last visit: 8/2/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already published in the following thread WHER I CAN FIND COMGRAPH PROGRAM AND HOW I CAN SETUP ON THE PG 730?. Best regards O_Moderator |
Follow us on