1/23/2007 3:33 PM | |
Joined: 4/24/2006 Last visit: 6/19/2024 Posts: 8684 Rating:
|
Hi bram-- If I understand it, when power goes off the Pnoz and then back on. Profibus is functioning? Have you seen the following link: http://support.automation.siemens.com/WW/view/en/19732230 In hardware configuration, you can double click on CPU and go to tab Startup. Here are some monitoring times, have you already make them bigger? Best regards, Wizard |
8/27/2010 9:08 AM | |
Joined: 6/20/2006 Last visit: 2/4/2024 Posts: 3 Rating:
|
I have the same problem. Did anyone find a solution? Best regards |
8/30/2010 1:38 PM | |
Joined: 8/25/2005 Last visit: 6/12/2024 Posts: 1162 Rating:
|
Hello jurc, If you didn't get information which are detailed enough from the integrated diagnostic tools please have a look at the telegrams which are send at the bus. The software Amprolyzer could be used for example to monitor the communication. It would be very interesting to analyse this information. Good luck Sabine |
Follow us on