8/19/2011 10:09 PM | |
Joined: 5/18/2006 Last visit: 10/21/2020 Posts: 170 Rating: (64) |
What are you trying to do? If you just want to build standard process graphics you should insert them (pictures, 1 per folder)in the plant view of SIMATIC Manager under the appropriate plant hierarchy folder. Compile the OS with Picture Tree option selected. This builds you navigation to these SIMATIC Manager inserted pictures. All you need to do is modify those pictures that you added. You should not modifiy any pictures provided with the PCS 7 Product (unless you really know what you are doing). PCS 7 product pictures all begin with an '@' (i.e. @PCS&Typicals.com). See PCS 7 Compendium Part A for description on how to configure a PCS 7 System (from CPU up through HMI). cabreytj |
Follow us on