Industry Online Support
Technical Forum
8/12/2011 9:04 AM | |
Posts: 51 Rating: (1) |
Hello! I have a S7-200 system6ES7214-1BD22-0XB0 and a TD200 operator panel. I dont know what cable there is between them (se the picture) but I want to extend the cable to 20 meter. I want to use a standard siemens profibus cable and connectors instead, is that possible? As I remember it, there is no problem to use profibus cable and connector when you use MPI, and max length is 50m, so 20m should work? Am I right? But I dont know what communication there is, could it be PPI? (never worked with that). If there is PPI, can I still use a profibus cable and profibus connector 6ES7972-0BB42-0XA0? I just want to move the TD200 20 meters away, I dont want to "go in" and change parameters etc. |
Last edited by: Pontus at: 8/12/2011 9:06 AM |
|
8/12/2011 11:12 AM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
HI Pontus, I have used the Profinus Cable & Connector with TD 200 Communication, it is working also. I dont want to "go in" and change parameters etc. ? Let me know what you mean to say. |
Ammy |
|
Follow us on